DOCA0105EN-09

Digital Outputs

Digital Output Register Mapping

Each digital output description is made up of 60 registers. The order and the description of the digital outputs 2 and 3 are the same as those of digital output 1.

IO Module

Digital Output Number

Digital Output Addresses

Digital Output Registers

IO 1

O1

0x3849–0x3884

14410–14469

O2

0x3885–0x38C0

14470–14529

O3

0x38C1–0x38FC

14530–14589

IO 2

O1

0x4401–0x443C

17410–17469

O2

0x443D–0x4478

17470–17529

O3

0x4479–0x44B4

17530–17589

Digital Output 1 Registers of IO 1

The order and the description of the digital output 1 registers of IO 2 are the same as those of IO 1:

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3849

14410

R

INT16U

Quality of each bit of register 14411:

  • 0 = Invalid

  • 1 = Valid

0x384A

14411

R-WC

INT16U

0

Reserved

1

Digital output status:

  • 0 = OFF

  • 1 = ON

R

2

Digital output forced status:

  • 0 = Unforced

  • 1 = Forced

3–15

Reserved

0x384B–0x384E

14412–14415

R

DATETIME

Timestamp for the last output transition:

  • Last rising edge if output is configured as NO (normally open contact)

  • Last falling edge if output is configured as NC (normally closed contact)

0x384F–0x3850

14416–14417

Reserved

0x3851–0x3852

14418–14419

R

INT32U

1-4294967294

Output counter

This counter increments for each rising edge of the output.

0x3853–0x3856

14420–14423

R

DATETIME

Timestamp of the last reset for the output counter

0x3857–0x386E

14424–14447

R

OCTET STRING

Digital output identification coded over 45 ASCII characters

0x386F

14448

R

INT16U

0–2

Output operating mode(1):

  • 0 = Non-latching (factory setting)

  • 1 = Latched

  • 2 = Time delayed non-latching

0x3870

14449

R

s

INT16U

0–65534

On time for time delayed non-latching mode value(1)

The time for the output to remain energized when the output is in time delayed non-latching mode

(Factory setting = 0)

0x3871

14450

R

INT16U

0–1

Output contact type(1):

  • 0 = NO (normally open, factory setting)

  • 1 = NC (normally close)

0x3872

14451

R

INT16U

0–2

Indicates On/Off state of the discrete output when any fall back condition occurs(1):

  • 0 = OFF (factory setting)

  • 1 = ON

  • 2 = Freeze

0x3873–0x3874

14452–14453

R

INT32U

1-4294967294

Output counter threshold value(1)

Factory setting = 5000

0x3875

14454

R-WC

INT16U

0–2

Simple command for output(1):

  • 0 = No command

  • 1 = OFF

  • 2 = ON

Valid if simple commands are enabled(2).

0x3876–0x3884

14455–14469

Reserved

(1) Value set using the EcoStruxure Power Commission software.

(2) Simple commands are enabled by factory setting. The simple commands can be disabled by using the command Enable/Disable commands.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?