DOCA0105EN-09

Measurement Set and Reset Commands

List of Commands

The following table lists the measurement set and reset commands, their corresponding command codes, and user profiles:

Command

Command code

User profile

Reset minimum/maximum values and energies Reset Minimum/Maximum Values and Energies

46728

Administrator or Operator

Reset Minimum/Maximum Values and Energies

To reset minimum/maximum values and energy, set the command registers in the following way:

Address

Register

Unit

Type

Range

Bit

Description

0x1F3F

8000

INT16U

46728

Requested command code

0x1F40

8001

INT16U

12

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

0

Reset min-max current

1

Reset min-max voltage

2

Reset min-max power

3

Reset min-max power factor and cosφ

4

Reset min-max THD (% fund)

5

Reset peak current demand

6

Reset peak power demand

7

Reset min-max frequency

8

Reserved

9

Reset all energies

10–15

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.