DOCA0122EN-11

HMI - Human-machine interface

Refers to the display screens on the front face of a device that an operator can use to read information or configure the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?