DOCA0122EN-11

IFE server

IFE Ethernet switchboard server that can be connected to more than one MasterPacT MTZ circuit breaker. With this module, the circuit breakers are accessible over an Ethernet network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.