DOCA0122EN-11

IFE interface

IFE Ethernet interface for one circuit breaker that can be connected to one MasterPacT, ComPacT, or PowerPacT circuit breaker. With this module, the circuit breaker is accessible over an Ethernet network. Access to the IFE interface webpages and IFE FTPS server is authorized depending on the Role-Based Access Control (RBAC) mechanism.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.