DOCA0122EN-11

Identifying and Protecting Sensitive and Critical Information and Operations

Overview

When planning and designing an operational technology network, it is important to identify information that is critical or sensitive for your operations. Once identified, this information must be protected.

As a general principle:

  • Critical information includes data and operations accessible through the MasterPacT, ComPacT, and PowerPacT IMU (for example, status of the circuit breaker, trip, or open/close command).

  • Sensitive information includes any information that can be used to access your installation and your operational technology network (for example, passwords or access codes for equipment or for locked rooms).

It is your responsibility to determine how this information could be analyzed and used against your organization best interest.

Information About the Enterprise Communication Network

Sensitive information that can be used to access your installation and control network includes:

  • Your system architecture

  • IP addresses or MAC addresses of networked communicating devices

  • Port numbers used for Ethernet communication

  • User IDs and user passwords

This list is not exhaustive, and it is important to consider all information specific to your organization that can facilitate access to critical systems.

Access Control

An important part of cybersecurity consists in designing an effective access control policy. Access control consists in identifying groups of users or individual employees within your organization, and determining the type and the level of access they need to carry out their jobs effectively.

Summary of Information and Operations Accessible Through Each Access Path

Depending on the communication interface or the communication path used to access the MasterPacT, ComPacT, and PowerPacT intelligent modular unit (IMU), the information and control operations available are different.

The following table summarizes access to information and control operations through the MasterPacT MTZ IMU with MicroLogic X control unit:

Information and control operations

Local access

Remote access

MicroLogic X HMI

FDM121 display

NFC

Bluetooth Low Energy technology

USB

Ethernet / Modbus-SL

Data monitoring

Read

Read

Read

Read

Read

Read

Protection settings

Read/Write

Read

Read

Read/Write

Read/Write

Read/Write

Other settings

Read/Write

Read

Read

Read/Write

Read/Write

Read/Write

Open/Close/Reset

No

Yes

No

Yes

Yes

Yes

The following table summarizes access to information and control operations through the MasterPacT MTZ IMU with MicroLogic Active control unit:

Information and control operations

Local access

Remote access

MicroLogic Active HMI

FDM121 display

NFC

USB

Zigbee

Ethernet / Modbus-SL

Data monitoring

Read

Read

Read

Read

Read

Read

Protection settings

Read/Write

Read

Read

Read/Write

No

Read

Other settings

Read/Write

Read

Read

Read/Write

Read

Read

Open/Close/Reset

No

Yes, in Auto Local control mode only

No

Yes

No

Yes, in Auto Remote control mode only

The following table summarizes access to information and control operations through the MasterPacT NT/NW, ComPacT NS, and PowerPacT P- and R-Frame IMU:

Information and control operations

Local access

Remote access

MicroLogic HMI

FDM121 display

Test port

Ethernet / Modbus-SL

Data monitoring

Read

Read

Read

Read

Protection settings

Read/Write

Read

Read/Write

Read/Write

Other settings

Read/Write

Read

Read/Write

Read/Write

Open/Close/Reset

No

Yes

Yes

Yes

The following table summarizes access to information and control operations through the ComPacT NSX and PowerPacT H-, J-, and L-Frame IMU:

Information and control operations

Local access

Remote access

MicroLogic HMI

FDM121 display

Test port

Ethernet / Modbus-SL

Data monitoring

Read

Read

Read

Read

Protection settings

Read/Write

Read

Read/Write

Read/Write

Other settings

Read/Write

Read

Read/Write

Read/Write

Open/Close/Reset

No

Yes

Yes

Yes

For information on protecting each communication interface and access path, see the recommendations for local access or for remote access, as appropriate.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?