Purchasing and Installing Digital Modules (MasterPacT MTZ)
Overview
Digital Modules are optional modules that expand the features available across the range of MicroLogic X control units. They can be purchased along with the MasterPacT MTZ circuit breaker in the initial order or at a later date by contacting the Customer Care Center (CCC).
Digital Modules designed for the MicroLogic X control unit are digitally signed for added security using the Schneider Electric public key infrastructure (PKI). The PKI helps to ensure both the authenticity and integrity of these downloads. The Digital Modules must be installed using EcoStruxure Power Commission software.
Cybersecurity Recommendations for Installing Digital Modules
WARNING |
|---|
|
RISK OF UNINTENDED OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
When installing Digital Modules for the MicroLogic X control unit, it is recommended to:
-
Install Digital Modules following accepted operational technology (OT) practices such as testing on a non-production environment for validation before installing and deploying them in your production system.
-
Only use the latest version of EcoStruxure Power Commission software to download and install Digital Modules.
-
Harden the PCs used to download Digital Modules and to install them following the most recent vendor guidelines for the operating system.
You must use only EcoStruxure Power Commission software to install Digital Modules for the MicroLogic X control unit.
EcoStruxure Power Commission software plays an important part in helping ensure the integrity of your operational technology network. Use only the latest version of EcoStruxure Power Commission software to install Digital Modules because it is the only software that can provide the following benefits:
-
When you update the firmware of a device of the IMU using EcoStruxure Power Commission software over a USB connection or Ethernet connection, the digital signature of the firmware update is automatically verified.
-
When you upload a Digital Module to the MicroLogic X control unit using EcoStruxure Power Commission software over a USB connection, the digital signature of the Digital Module is automatically verified.
The automatic verifications done by EcoStruxure Power Commission software rely entirely on the validity of the public certificate used.
Refer to DOCA0144EN MasterPacT MTZ - MicroLogic X Control Unit - Firmware Release Notes for detailed procedures explaining how to download and install Digital Modules.
WARNING