DOCA0122EN-11

IMU - Intelligent modular unit

The circuit breaker with its internal communicating components (MicroLogic trip unit or control unit) and external ULP modules (IO module), connected to one communication interface is called an intelligent modular unit (IMU).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.