DOCA0122EN-11

BSCM Modbus SL/ULP module

The BSCM Modbus SL/ULP module with commercial reference LV434220 is a Breaker Status Control Module that can be used to communicate data via Modbus Serial Line communication network or via ULP communication network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.