DOCA0122EN-11

Cybersecurity Recommendations for Disposal or Decommissioning

The EIFE and IFE interfaces and IFE server contain confidential information configured during commissioning, recent data values and logs. For example, this information can include passwords or measured power consumptions.

It is required to perform a factory reset before disposing of the EIFE or IFE interface, or IFE server. For more information, refer to the relevant user guide for your interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.