DOCA0122EN-11

Recommendations for Protecting Access Through Zigbee Wireless Technology (MasterPacT MTZ)

Zigbee Version

MicroLogic Active AP/EP control units are certified for Zigbee 3.0.

Functions Accessible Through Zigbee Wireless Technology

Using Zigbee wireless communication, you can monitor data from the MicroLogic Active AP/EP control unit from a Panel Server Advanced (PAS800), Panel Server Universal (PAS600) or Panel Server Entry (PAS400).

Data transferred over Zigbee wireless technology is encrypted using AES 128-bit encryption algorithm.

NOTE: Zigbee wireless technology is not available in MicroLogic X control units.

Prerequisites for Establishing a Zigbee Connection

TBC@Osman+Zigbee experts: clarify the use of Zigbee ID vs Zigbee installation code here, on go2se page and on the HMI

The prerequisites to establishing a Zigbee connection are:

  • The Panel Server must be turned on.

  • The MicroLogic Active AP/EP control unit and Panel Server must be in close proximity.

  • For selective pairing, you must provide the Zigbee ID, displayed on the Go2SE landing page or the MicroLogic Active display screen.

For detailed procedures on how to establish a Zigbee connection, see the Commissioning chapter of the MasterPacT MTZ Circuit Breaker with MicroLogic Active Control Unit User Guides.

General Recommendations for Protecting Access Through Zigbee Wireless Technology

To protect access to functions accessible through Zigbee wireless technology, it is recommended to:

  • Install the MasterPacT MTZ circuit breaker in a locked area so that only authorized personnel can access the MicroLogic Active control unit.

  • Keep that area locked at all times.

  • Give the key or access code to authorized personnel only.

For further information on protecting access to the MasterPacT MTZ circuit breaker, refer to Implementing a Restricted Access Policy.

Recommendations for Using Zigbee Wireless Technology

Zigbee wireless communication is vulnerable to disruption by unauthorized radio emissions in the operating environment. To protect access to functions accessible through Zigbee wireless communication, it is recommended that:

  • The MicroLogic Active AP/EP control unit is not connected to malicious networks.

  • The Zigbee network is checked regularly to ensure that all devices are valid.

  • The Zigbee network is repaired if any device is invalid.

  • The commissioning of Zigbee wireless devices is done in a place secure from rogue radio transmitters, such as an administrator room.

  • Pairing must be done only when necessary and in a secure area.

Recommendations for Using Panel Server

Refer to the Cybersecurity Recommendations chapter of DOCA0172•• EcoStruxure Panel Server - User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.