DOCA0122EN-11

IEC 61850 Protocol

A standard for communication networks and systems in substations. Based on Ethernet protocol, it is a standardized method of communication developed to support integrated systems, composed of multi-vendor, self-describing Intelligent Electronic Devices (IEDs). These systems are networked together to perform real-time protection, control, measurement, and monitoring functions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.