DOCA0122EN-11

EIFE interface

Embedded Ethernet interface that is an optional module of the MasterPacT MTZ drawout circuit breaker. With this module, the circuit breaker is accessible over an Ethernet network. Access to the EIFE interface webpages and EIFE FTPS server is authorized depending on the Role-Based Access Control (RBAC) mechanism.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.