DOCA0122EN-11

Cybersecurity Recommendations for System Design, Planning and Installation

Overview

This part provides important information to consider during the design, planning, and installation phases of an operational technology (OT) network that includes the MasterPacT, ComPacT, and PowerPacT intelligent modular unit (IMU). The recommendations and guidelines in this part help to build a secure operating environment.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?