DOCA0122EN-11

Why Cybersecurity Is Relevant for MasterPacT, ComPacT, and PowerPacT Circuit Breakers

Overview

The MasterPacT, ComPacT, and PowerPacT circuit breaker is a key component of any plant or equipment because it controls the power supply to the process, provides electrical protection, and delivers critical information.

MasterPacT, ComPacT, and PowerPacT circuit breakers with communication features also provide 24/7 access to real-time control functions and to monitoring data. These features bring greater efficiency and flexibility in managing your electrical distribution system. However, they may be subject to cyber attacks.

MasterPacT MTZ Circuit Breaker with MicroLogic X Control Unit Operating Environment

The following figure shows the various ways of communicating with the MicroLogic X control unit of the MasterPacT MTZ circuit breaker.

USB

ULP

Ethernet

Bluetooth® wireless technology

Wi-Fi

MasterPacT MTZ intelligent modular unit (IMU)

Operational technology (OT) network

Public Internet

The MasterPacT MTZ intelligent modular unit (IMU) represents the circuit breaker, the MicroLogic X control unit, and the associated ULP modules, communication interface, and IO modules.

To communicate with the MasterPacT MTZ circuit breaker through its MicroLogic X control unit, the following communication paths are available:

  • MicroLogic X human-machine interface (HMI)

  • FDM121 front display module for one circuit breaker

  • Wireless NFC connection from a smartphone

  • Wireless Bluetooth Low Energy connection from a smartphone

  • Connection to the mini type B USB port of the MicroLogic X control unit from:

    • A PC running EcoStruxure™ Power Commission software

    • A smartphone running the EcoStruxure Power Device app

  • Ethernet (Modbus TCP/IP or IEC 61850 protocols) connection through the operational technology (OT) network when the IFE or EIFE interface, or IFE server is present

  • Modbus-SL connection through the operational technology (OT) network when the IFM interface is present

MasterPacT MTZ Circuit Breaker with MicroLogic Active Control Unit Operating Environment

The following figure shows the various ways of communicating with the MicroLogic Active control unit of the MasterPacT MTZ circuit breaker.

USB

NFC

Wi-Fi

Zigbee

MasterPacT MTZ intelligent modular unit (IMU)

Operational technology (OT) network

Public Internet

A Panel Server webpages

B EcoStruxure Power Monitoring Expert (PME) software

C EcoStruxure Power Operation (PO) software

D POI Plus, industrial workstation with energy management software

The MasterPacT MTZ intelligent modular unit (IMU) represents the circuit breaker, the MicroLogic Active control unit, and the associated ULP modules and the communication interface.

To communicate with the MasterPacT MTZ circuit breaker through its MicroLogic Active control unit, the following communication paths are available:

  • MicroLogic Active human-machine interface (HMI)

  • FDM121 front display module for one circuit breaker

  • Wireless NFC connection from a smartphone

  • Connection to the USB-C port of the MicroLogic Active control unit from:

    • A PC running EcoStruxure™ Power Commission software

    • A smartphone running the EcoStruxure Power Device app

  • Wireless Zigbee connection to a Panel Server for MicroLogic Active AP/EP control units.

  • Ethernet (Modbus TCP/IP protocol) connection through the operational technology (OT) network when the IFE or EIFE interface, or IFE server is present

  • Modbus-SL connection through the operational technology (OT) network when the IFM interface is present

MasterPacT NT/NW, ComPacT NS, and PowerPacT P- and R-Frame Circuit Breaker Operating Environment

The following figure shows the various ways of communicating with the MicroLogic trip unit of the circuit breaker.

USB

ULP

Ethernet

Intelligent modular unit (IMU)

Operational technology (OT) network

Public Internet

The intelligent modular unit (IMU) represents the MasterPacT NT/NW, ComPacT NS, or PowerPacT P- or R-frame circuit breaker, the MicroLogic trip unit, and the associated ULP modules, communication interface, and IO modules.

To communicate with the circuit breaker through its MicroLogic trip unit, the following communication paths are available:

  • MicroLogic human-machine interface (HMI)

  • FDM121 front display module for one circuit breaker

  • Connection to the MicroLogic trip unit from a PC running EcoStruxure Power Commission software through the Service interface

  • Ethernet (Modbus TCP/IP protocol) connection through the operational technology (OT) network when the IFE interface or IFE server is present

  • Modbus-SL connection through the operational technology (OT) network when the IFM interface is present

ComPacT NSX, and PowerPacT H-, J- and L-Frame Circuit Breaker Operating Environment

The following figure shows the various ways of communicating with the MicroLogic trip unit of the circuit breaker.

USB

ULP

Ethernet

Intelligent modular unit (IMU)

Operational technology (OT) network

Public Internet

The intelligent modular unit (IMU) represents the ComPacT NSX or PowerPacT H-, J- or L-Frame circuit breaker, the MicroLogic trip unit, and the associated ULP modules, communication interface, and IO modules.

To communicate with the circuit breaker through its MicroLogic trip unit, the following communication paths are available:

  • MicroLogic human-machine interface (HMI)

  • FDM121 front display module for one circuit breaker

  • Connection to the MicroLogic trip unit from a PC running EcoStruxure Power Commission software through the Service Interface or USB maintenance interface

  • Ethernet (Modbus TCP/IP protocol) connection through the operational technology (OT) network when the IFE interface or IFE server is present

  • Modbus-SL connection through the operational technology (OT) network when the IFM interface or BSCM Modbus SL/ULP module is present

System Vulnerability to Cyber Attacks

Each of the communication paths listed above represents a potential vulnerable point in your system if security measures are not put in place. This guide provides guidelines to help secure these communication paths to avoid intentional attacks or accidental misuse.

The following security features are intended to mitigate the inherent threats which are linked to the usage of IFE and EIFE interfaces, IFE server, and MasterPacT, ComPacT, and PowerPacT devices in an Operational Technology (OT) environment.

Security Features Provided

The following cybersecurity functions are supported by MasterPacT, ComPacT, and PowerPacT IMUs:

  • User account management:

  • Access code protection

  • Configurable security services and settings

  • Firmware update mechanism

  • Secure machine-to-machine communication via Modbus TCP/TLS (on IFE and EIFE interfaces, and IFE server)

  • Security logs in Syslog format or CSV format (on IFE and EIFE interfaces, and IFE server)

These features provide security capabilities which contribute towards protecting the product from potential security threats that could:

  • Disrupt the product operation (availability)

  • Modify information (integrity)

  • Disclose confidential information (confidentiality)

Security Features Comparison Between IFE/EIFE Interface and IFE Server

The following table provides a comparison between the available security features in these firmware versions:

  • IFE/EIFE interface with firmware versions 004.•••.••• and 005.•••.•••

  • IFE server with firmware version 003.•••.•••

  • IFE server with firmware version 005.•••.•••

Schneider Electric recommends that you update the firmware version of the IFE/EIFE interface and IFE server to benefit from the latest features.

Features

Availability

Default state of available features

EIFE Interface (LV851001)

IFE Interface (LV434001)

IFE Server (LV434002)

(firmware version 003.•••.•••)

IFE Server (LV434002)

(firmware version 005.•••.•••)

HTTP

Yes

Yes

Yes

Enabled

HTTPS

Yes

No

Yes

Enabled

FTP-Server

Yes

Yes

Yes

Disabled

FTP-Client

Yes

Yes

Yes

Disabled

FTPS

Yes

No

Yes

Enabled

NTP

Yes

No

Yes

Disabled

SNTP

No

Yes

No

Disabled

RSTP

Yes

No

Yes

Disabled

Modbus TCP

Yes

Yes

Yes

Enabled

Modbus Secure

Yes

No

Yes

Disabled

RBAC

Yes

No

Yes

Enabled

IEC 61850

Yes

No

Yes

Disabled

Syslog

Yes

No

Yes

Enabled

SMTP

Yes

Yes

Yes

Disabled

IPv6 support and DPWS discovery

Yes

No

Yes

Enabled

SNMP

Yes

Yes

Yes

Disabled

Time to upgrade the firmware

4 minutes approximately

16 minutes approximately

4 minutes approximately

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.