DOCA0122EN-11

ULP connectivity

ULP is a fast communication link dedicated to circuit breaker monitoring and control. It connects the circuit breaker to an Ethernet interface or to an IO module. ULP operates at a speed of 1 Mb/s and is plug and play.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.