DOCA0122EN-11

PacT Series Master Range

Future-proof your installation with Schneider Electric’s low-voltage and medium-voltage PacT Series. Built on legendary Schneider Electric innovation, the PacT Series comprises world-class circuit breakers, switches, residual current devices and fuses, for all standard and specific applications. Experience robust performance with PacT Series within the EcoStruxure-ready switchgear, from 16 to 6300 A in low-voltage and up to 40.5 kV in medium-voltage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.