DOCA0161EN-02

Connection terminal

Flat copper surface, linked to the conducting parts of the device, and to which power connections are made using bars, connectors or lugs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.