DOCA0161EN-02

Extented rotary handle

Rotary handle with an extended shaft to control devices installed at the rear of switchboards. It has the same characteristics as direct rotary handles. It offers multiple locking possibilities using a padlock or a door interlock.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.