DOCA0161EN-02

Electrical durability

With respect to its resistance to electrical wear, equipment is characterized by the number of on-load operating cycles, corresponding to the service conditions given in the relevant product standard, which can be made without replacement.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.