DOCA0161EN-02

Thermal protection

Protection against over currents following an inverse time curve I2t = constant, which defines the maximum permissible temperature rise for the motor. Tripping occurs after a time delay that decreases with increasing current.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.