DOCA0161EN-02

SDTAM Thermal Fault Module

Introduction

Use the SDTAM thermal fault module to manage tripping due to overload.

The SDTAM thermal fault module receives data from the trip unit through an optical link and makes available two outputs assigned to:

  • Overload indication

  • Motor contactor control

Description

A Output terminals

B SDTAM thermal fault module

C Operating mode adjustment dial

Characteristics

The characteristics of the SDTAM thermal fault module outputs are:

  • Voltage: 24–415 Vac/Vdc

  • Current:

    • Active outputs: 80 mA maximum

    • Idle outputs: 0.25 mA

Installation

The slots used to install the SDTAM thermal fault module depend on the device.

TeSys GV5

TeSys GV6

The SDTAM thermal fault module uses the same slot as:

  • MN/UVR undervoltage trip release, MX/SHT shunt trip, or OF1 auxiliary contact in a TeSys GV5 device.

  • MN/UVR undervoltage trip release or MX/SHT shunt trip in a TeSys GV6 device.

Wiring diagram

Connect the SDTAM thermal fault module and the two outputs in strict accordance with the wiring diagram.

The diagram is shown with circuits de-energized, all devices open, connected and charged and relays in normal position.

Item

Description

SD1, SD3

Thermal fault module input power supply

SD2

Overload fault signal output. This output maintains its state until reset.

SD4

Contactor control output

KM1

LC1D or LC1F contactor

KA1

CA2 or CAD-type control relays

Output Assignment

Output 1 (SD2/OUT1): normally open, indicates thermal faults.

Output 2 (SD4/OUT2): normally closed, opens the contactor KM1.

Outputs are activated 400 ms before the device trips in the case of:

  • Overload or thermal protection

  • Phase-unbalance protection

Contactor Control

Contactor control by the output 2 signal (SD4/OUT2) optimizes continuity of service and provides the following additional benefits:

  • Lower risk of motor deterioration.

  • Activation of the output indicates that the application is not working normally. Abnormal operation is not the result of an anomaly or internal fault in the motor-feeder.

  • The cause of this abnormal operation can be temporary (for example, a voltage drop causing an overly long starting time).

When the cause of the overload or unbalance has disappeared, the equipment can be powered up again.

NOTE: To control a contactor with a consumption exceeding 80 mA, it is necessary to provide a control relay.

Operating Modes

The SDTAM thermal fault module incorporates an auto-reset delay setting dial.

To return the outputs to their initial state following activation:

  • Manual (SDTAM dial in the OFF position) after canceling the module power supply.

  • Automatic (SDTAM dial on one of the time delay adjustment settings) following a time delay (set from 1 to 15 minutes to allow for the motor cooling time).

Item

Description

I

Motor current

Output 1

SDTAM overload fault signal output

Output 2

SDTAM contactor control output

KM1

Motor contactor

Q

TeSys GV5 / GV6 device

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.