DOCA0161EN-02

Direct rotary handle

This is a control handle for the circuit breaker. It has the same three positions I (ON), O (OFF) and TRIP as the toggle control. It provides IP40 and IK07 protections. It maintains suitability for isolation and offers optional locking using a padlock.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.