DOCA0161EN-02

Reflex Tripping

Introduction

TeSys GV5 / GV6 devices incorporate the exclusive reflex-tripping system.

This system breaks very high fault currents.

The device is mechanically tripped via a “piston” actuated directly by the short-circuit.

For high short-circuits, this system provides a faster break, thereby ensuring discrimination.

Reflex-tripping curves are exclusively a function of the device rating.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.