DOCA0161EN-02

Ics: Service breaking capacity

Expressed as a percentage of Icu, it provides an indication on the robustness of the device under severe conditions. It is confirmed by a test with one opening and one closing/opening at Ics, followed by a check that the device operates correctly at its rated current.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.