DOCA0161EN-02

Starting current

Start-up of a three-phase, asynchronous motor is characterized by:

  • A high inrush current, approximately 14 x In for 10 to 15 ms

  • A starting current, approximately 7.2 x In for 5 to 30 seconds

  • Return to the rated current after the starting time

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.