DOCA0161EN-02

Indication Contacts

Introduction

Use indication contacts to view the status of the device remotely. One indicator contact model provides OF, SD, or SDE indication functions. The position of the contact inside the case determines the function.

Indication contacts are located under the front face of the device, in a compartment isolated from the power circuits. There are two types of indication contact:

  • Standard contact with spring terminals

  • Low-level contact with screw terminals

For more information about installation, consult the instruction sheet on the Schneider Electric website: NNZ4314501 Indication Contacts.

Standard and Low-Level Contacts

Standard and low-level contacts are the common point changeover type.

NC Normally Closed contact

NO Normally Open contact

The following table describes the operation of standard and low-level volt-free contacts:

Name

Definition

OF open/close indication contact

The OF contact indicates the position of the main contacts of the device (open or closed).

SD trip indication contact

The SD contact indicates that the device has tripped due to:

  • Operation of the push-to-trip button

  • Operation of the MN/UVR undervoltage trip release or MX/SHT shunt trip

  • Overload or thermal protection

  • Short-time protection

  • Instantaneous protection

  • Phase-unbalance protection

SDE electrical fault contact

The SDE contact indicates that the device has tripped on an electrical fault due to:

  • Overload or thermal protection

  • Short-time protection

  • Instantaneous protection

  • Phase-unbalance protection

Operation of the Indication Contacts

The following table shows the position of the indication contacts for each position of the handle and main contacts.

Name

Contact number

Position of the handle and contacts

Handle position

Device status

OFF

ON

Tripped on electrical fault *

Tripped by MN/UVR, MX/SHT or push-to-trip protection

Main contact position

Open

Closed

Open

Open

OF auxiliary contact position

•1–•2

Closed

Open

Closed

Closed

•1–•4

Open

Closed

Open

Open

SD auxiliary contact position

•1–•2

Closed

Closed

Open

Open

•1–•4

Open

Open

Closed

Closed

SDE auxiliary contact position

•1–•2

Open

Open

Closed

Open

•1–•4

Closed

Closed

Open

Closed

Wiring Diagram

The diagram is shown with circuits de-energized, all devices open, connected, and charged, and relays in normal position.

Indication contacts

Description

OF4/OF3/OF2/OF1

Device ON/OFF indication contacts

SDE

Electrical fault trip indication contact (short-circuit, overload, phase-unbalance)

SD

Trip indication contact

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.