DOCA0161EN-02

Trip Unit Description

Introduction

The trip unit is suitable for protecting motor-feeders in standard applications.

The thermal trip curves are calculated for self-ventilated motors.

The adjustment dials and indications are located on the front face.

Description

TeSys GV5 trip unit

TeSys GV6 trip unit

A Indication LEDs

B Phase-unbalance

C Seal for setting cover

D Setting range

E Instantaneous protection pickup (Ii)

F Tripping curve

G Adjustment dial for the short-time protection pickup (Isd)

H Trip class setting

I Adjustment dial for the overload or thermal protection pickup (Ir)

Indication LEDs

Indication LEDs on the front of the trip unit indicate its operational state.

Indication LED

Description

Green READY LED

Blinks slowly when the electronic trip unit is ready to provide protection.

Red ALARM LED

Overload temperature alarm LED: Shows a steady light when the thermal image of the motor exceeds 95% of the Ir setting.

The indication LEDs function for device load currents above 30 A.

Protection Functions

The following figure and table define the protection functions performed by the trip unit:

Item

Parameter

Description

Adjustable

Default setting

SDTAM activation

A

Ir

Overload or thermal protection pickup

Yes

0.4 x In

Yes

B

Class

Trip class

Yes

10

Yes

C

Isd

Short-time protection pickup

Yes

13 x Ir

No

D

tsd

Short-time protection time delay

No

0.1 s

No

E

Ii

Instantaneous protection pickup

No

17 x In

No

Iunbal

Phase-unbalance protection pickup

No

30%

Yes

tunbal

Phase-unbalance protection time delay during startup

No

0.7 s

Yes

Phase-unbalance protection time delay in steady state

No

4 s

Yes

Each function is reviewed in detail on the following pages.

Setting the Protection

Set the overload or thermal protection pickup (Ir), the short-time protection pickup (Isd), and trip class (Class) by using the dials on the device.

Reflex Tripping

The system of reflex protection breaks very high fault currents by mechanically tripping the device with a piston actuated directly by the pressure produced in the device from a short-circuit. This piston operates the opening mechanism, resulting in ultra-fast device tripping.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.