DOCA0161EN-02

In: Rated current

The rated current corresponds to the current that the device can carry continuously with the contacts closed and without abnormal temperature rise.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.