DOCA0161EN-02

Electrical Auxiliary Devices

Summary of Electrical Auxiliary Devices

The following table shows electrical auxiliary devices that can be added to devices. They can be installed on site. For more information, refer to TeSys Motor Control and Protection Components Catalog.

Electrical auxiliary device

Use

OF auxiliary contact

View the on/off status of the device remotely.

SD auxiliary contact

View the trip status of the device remotely.

SDE auxiliary contact

Indicate that the device has tripped on an electrical fault.

MN/UVR undervoltage trip release

Trip the device when the control voltage drops below a tripping threshold.

MX/SHT shunt trip

Send an electrical trip command remotely to trip the device.

SDTAM thermal fault module

Provide alarm and fault differentiation.

Slots for Electrical Auxiliary Devices on TeSys GV5 Devices

The following table shows the possible slots for electrical auxiliary devices mounted in the case.

Electrical auxiliary device

Slot

A

B

C

D

E

OF1 auxiliary contact

OF2 auxiliary contact

SD auxiliary contact

SDE auxiliary contact (with addition of the optional SDE adapter)

MN/UVR undervoltage trip release

MX/SHT shunt trip

SDTAM thermal fault module

NOTE: It is not possible to install all the accessories at the same time in one device. For example, SDTAM thermal fault module uses the same slot as MN/UVR undervoltage trip release or MX/SHT shunt trip.

Slots for Electrical Auxiliary Devices on TeSys GV6 Devices

The following table shows the possible slots for electrical auxiliary devices mounted in the case.

Electrical auxiliary device

Slot

A

B

C

D

E

F

G

H

OF1 auxiliary contact

OF2 auxiliary contact

OF3 auxiliary contact

OF4 auxiliary contact

SD auxiliary contact

SDE auxiliary contact (with embedded SDE adapter)

MN/UVR undervoltage trip release

MX/SHT shunt trip

SDTAM thermal fault module

NOTE: It is not possible to install all the accessories at the same time in one device. For example, SDTAM thermal fault module uses the same slot as MN/UVR undervoltage trip release or MX/SHT shunt trip.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?