DOCA0108EN-03

Modbus Functions

General Description

The Modbus protocol offers a number of functions that are used to read or write data over the Modbus network. The Modbus protocol also offers diagnostic and network-management functions.

Only the Modbus functions handled by the VigiPacT relays are described here.

Functions

The following functions are available:

Function Code

Subfunction Code

Name

Description

1 (0x01)

Read coils

Read output bits

2 (0x02)

Read discrete inputs

Read input bits

3 (0x03)

Read holding registers

Read n registers

5 (0x05)

Write single coil

Write 1 bit

6 (0x06)

Write single register

Write 1 register

16 (0x10)

Write multiple registers

Write n registers

43 (0x2B)

14 (0x0E)

Read device identification

Read the identification data of the server

Read Register Example

The following table shows how to read the measured current in the register 1005. The address of register 1005 is 1005-1 = 1004 = 0x03EC. The Modbus address of the Modbus server is 247 = 0xF7.

Client Request

Server Reply

Field Name

Example

Field Name

Example

Modbus server address

0xF7

Modbus server address

0xF7

Function code

0x03

Function code

0x03

Address of the register to read (MSB)

0x03

Data length in bytes

0x02

Address of the register to read (LSB)

0xEC

Register value (MSB)

0x12

Number of registers (MSB)

0x00

Register value (LSB)

0x34

Number of registers (LSB)

0x01

CRC (MSB)

0xXX

CRC (MSB)

0xXX

CRC (LSB)

0xXX

CRC (LSB)

0xXX

The content of register 1005 (address 0x03EC) is 0x1234 = 4660. Therefore the measured current is 4660 mA.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?