DOCA0108EN-03

Channel Detailed Registers

Overview

The relevant data for each of the 12 channels are gathered together in 20 registers:

  • 4 status and control registers

  • 6 measurements registers

  • 10 parameter registers.

Only the registers for channel 1 are described. The registers for the other channels are organized as for the channel 1.

Mapping of the Detailed Channel Registers

Address

Register

Description

0x03E8–0x03FB

1001–1020

Channel 1 registers

0x03FC–0x040F

1021–1040

Channel 2 registers

0x040E–0x0423

1041–1060

Channel 3 registers

0x0424–0x0437

1061–1080

Channel 4 registers

0x0438–0x044B

1081–1100

Channel 5 registers

0x044C–0x045F

1101–1120

Channel 6 registers

0x045E–0x0473

1121–1140

Channel 7 registers

0x0474–0x0487

1141–1160

Channel 8 registers

0x0488–0x049B

1161–1180

Channel 9 registers

0x049C–0x04AF

1181–1200

Channel 10 registers

0x04AE–0x04C3

1201–1220

Channel 11 registers

0x04C4–0x04D7

1221–1240

Channel 12 registers

Channel 1 Status and Control Registers

Address

Register

RW

Units

Type

Range

Factory

Saved

Bit

Description

0x03E8

1001

R

NA

BITMAP

NA

0x003F

No

Validity of each bit of Status - Ch1:

  • 0 = invalid

  • 1 = valid

0x03E9

1002

R

NA

BITMAP

NA

0x0000

No

 

Channel 1 status

0

Alarm

1

Pre-alarm

2

Alarm is memorized

3

Toroid is connected

4

Alarm relay is active

5

Pre-alarm relay is active

6–15

Reserved

0x03EA–0x03EB

1003–1004

R

Reserved

Channel 1 Measurement Registers

Address

Register

RW

Units

Type

Range

Factory

Saved

Description

0x03EC

1005

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 1

0x03ED

1006

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 1

0x03EE

1007

R

%

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 1

Channel 1 Parameter Registers

Address

Register

RW

Units

Type

Range

Factory

Saved

Description

0x03EF

1008

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 1

0x03F0

1009

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 1

0x03F1

1010

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 1

0x03F2

1011

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 1

0x03F3–0x03FB

1012–1020

R

BITMAP

0x0000

No

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?