DOCA0108EN-03

Parameter Modification

Overview

To modify the value of a parameter, follow either of the methods described below:

  • Select a value in a list.

  • Modify a numerical value, digit by digit.

Selecting a Value in a List

To select a value, use the menu buttons as described below:

Icons

Description

Allows to scroll up to select the desired value.

Allows to scroll down to select the desired value.

Allows to save the selected parameter value.

Allows to exit the current value selection.

Modifying a Numerical Value

The numerical value of a parameter is made up of digits from 0 to 9.

To modify the numerical value, use the menu buttons as described below:

Icons

Description

Allows to increase the numerical value.

Allows to decrease the numerical value.

Allows to:

  • confirm the new parameter value and to move to the next digit.

  • save the parameter once the last digit is set.

Allows to exit the current parameter entry.

NOTE: After entering the value if no button is pressed for 10 seconds then the parameter modification is cancelled. The current screen remains displayed.

Pressing Multiple Buttons

If multiple buttons are pressed simultaneously, no action is performed and the pressed buttons are ignored except for the password reset function (refer to Password Management (7/7)). Release the pressed buttons to press another button.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?