DOCA0108EN-03

Metering Menu (1/7)

Overview

The Metering menu displays the list of channels to which toroids are connected.

Press or to select the desired toroid from the list and then press to display the Metering screen of the selected toroid.

Metering Screen for Toroid Number 01

The figure displays the Metering screen for the toroid 01 with the earth-leakage current.

A

Alarm threshold value from 30 mA to 999 mA in mA and from 1 A to 30 A in A.

B

Selected toroid number.

C

Measured earth-leakage current of the toroid in mA or A and as percentage of alarm threshold value.

D

Maximum measured earth-leakage current from 10 mA to 60 A.

NOTE: If the earth-leakage current reaches the maximum measurable value, SAT is displayed instead of the value.

Resetting the Maximum Measured Earth-Leakage Current

To reset the maximum measured earth-leakage current in the Metering screen, press for 10 seconds and then release the button.

NOTE: After is pressed for 5 seconds, the display starts blinking. If released after 5 seconds, the reset is cancelled.
NOTE: The maximum measured earth-leakage current can be reset only in the Metering screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?