VigiPacT Registers
Identification and Status
|
Address |
Register |
RW |
Units |
Type |
Range |
Factory |
Saved |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0064– 0x0069 |
101–106 |
R |
NA |
STRING |
NA |
NA |
Yes |
– |
Serial number on 12 ASCII characters PPYYWWDnnnn with
|
|
0x006A–0x006E |
107–111 |
R |
NA |
STRING |
NA |
NA |
No |
– |
Boot software version on 9 ASCII characters Example: "000.000.001" |
|
0x006F |
112 |
R |
NA |
BITMAP |
NA |
NA |
No |
Reserved |
|
|
0x0070–0x0074 |
113–117 |
R |
NA |
STRING |
NA |
NA |
No |
– |
Exploit software version on 9 ASCII characters Example: "000.000.001" |
|
0x0075 |
118 |
R |
NA |
BITMAP |
NA |
NA |
No |
Reserved |
|
|
0x0076–0x007A |
119–123 |
R |
NA |
STRING |
NA |
NA |
Yes |
– |
Hardware version on 9 ASCII characters Example: "000.000.001" |
|
0x007B |
124 |
R |
NA |
BITMAP |
NA |
NA |
No |
Reserved |
|
|
0x007C |
125 |
R |
NA |
BITMAP |
NA |
0x00FF |
No |
– |
Validity of each bit of VigiPacT status: 0 = invalid 1 = valid |
|
0x007D |
126 |
R |
NA |
BITMAP |
NA |
0x0000 |
No |
– |
VigiPacT status |
|
0 |
Alarm relay is active |
||||||||
|
1 |
Pre-alarm relay is active |
||||||||
|
2 |
Test is on going |
||||||||
|
3 |
Test is passed and not reset |
||||||||
|
4 |
Test is failed and not reset |
||||||||
|
5 |
Toroid loss is active |
||||||||
|
6 |
RM12T multiplexer communication malfunction is active |
||||||||
|
7 |
VigiPacT internal malfunction is active |
||||||||
|
8–15 |
Reserved |
||||||||
|
0x007E–0x007F |
127–128 |
R |
– |
– |
– |
– |
No |
– |
Reserved |
|
0x0080–0x0081 |
129–130 |
R |
NA |
INT32U |
0 to 0xFFFFFFFF |
0 |
No |
– |
Number of frames not understood (Bad function code, Modbus exception, …) |