DOCA0108EN-03

Password Management (7/7)

Overview

A password entry is required to access or modify the following parameters:

  • Functional settings

  • Factory reset

  • Changing password

Changing the Password

Step

Action

1

Select Password from Home menu, and then press .

Result: Displays the password entry screen.

  • Press to select the digit. Pressing this button moves the selection from left to right.

  • Press to increase the value of the selected digit from 0 to 9.

  • Press to decrease the value of the selected digit from 9 to 0.

If the password is correct, then you can access the next screen.

If the password is incorrect, then the following screen is displayed for 10 seconds:

The previous screen is displayed if you press within 10 seconds or if you do not press any button.

2

The screen prompts to enter the new password if the entered old password is correct.

Enter the new password, and then press .

3

After entering the new password, the screen prompts to confirm the password.

Enter the password again.

Result: The message OK is displayed on the screen for 40 seconds if the new password and the confirmed password are same.

NOTE: If both the new password and the confirmed password are different, Not valid message is displayed for 40 seconds. Press within 40 seconds to change the password again. The screen prompts you to enter the new password again.

4

Press within 40 seconds to navigate to Home menu.

NOTE: The Metering screen is displayed if you do not press any button within 40 seconds.

Resetting the Password

If you forget the password, the password can be reset to the default password 0000. Contact your Schneider Electric technical support.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?