DOCA0108EN-03

VigiPacT Commands

Write Registers

Address

Register

RW

Units

Type

Range

Factory

Saved

Description

0xEA76

60023

RW

NA

INT16U

0–2

0x0000

Yes

Allow to test the device.

  • 0: no test

  • 1: test trip

  • 2 : test no trip

0xEA77

60024

RW

NA

INT16U

0–1

0x0000

Yes

Alarm reset

Bit 0 = 1: To reset the alarm

0xEA78

60025(1)

RW

NA

INT16U

1–247

0x00F7

Yes

Device Modbus address

0xEA79

60026(1)

RW

NA

INT16U

0–3

0x0002

Yes(2)

Communication speed setting

  • 0: 4800

  • 1: 9600

  • 2: 19200

  • 3: 38400

0xEA7A

60027(1)

RW

NA

INT16U

0–2

0x0002

Yes(2)

Communication parity setting

  • 0: None

  • 1: Odd

  • 2: Even

0xEA7B

60028(1)

RW

NA

INT16U

0–1

0x0000

Yes

  • 0: Autogo is not active

  • 1: Autogo is active

(1) Communication may be broken if the parameter is modified. Communication has to be re-established with the new value written in the register.

(2) Modifiable only if Autogo is not active.

Diagnostics Registers

Address

Register

RW

Units

Type

Range

Factory

Saved

Description

0xEA7C

60029

R

NA

INT16U

0x0000

Yes

Number of software resets.

0xEA7D

60030

R

NA

INT16U

0x0000

Yes

Number of times the device is powered on.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?