DOCA0108EN-03

Integration of VigiPacT RMH Relay in a Communicating Architecture

Communication Architecture

A

FDM128 Ethernet display for eight devices

B

IFE Ethernet switchboard server

C

IFM Modbus-SL interface for one circuit breaker

D

VigiPacT RMH monitoring relay

E

FDM121 ULP display for one circuit breaker

F

RJ45 male/male ULP cord

G

VigiPacT toroid (up to 12 toroids)

H

IO input/output application module for one circuit breaker

I

MasterPact NT/NW circuit breaker

J

Circuit breaker BCM ULP cord

K

NSX cord

L

ComPacT NSX/PowerPacT H-, J-, L-frame circuit breaker

M

VigiPacT RM12T multiplexer

N

Cable for Modbus SL-1x RJ45 and 1x Free wires

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?