DOCA0108EN-03

Product Information (5/7)

Overview

The Product information screen displays the commercial reference and the embedded firmware version.

The Product information screen displays the embedded software version, hardware version and commercial reference.

The figure shows the Product information screen.

Where,

  • LVXXXXXX displays the commercial reference of the VigiPacT RMH relay.

  • XXX.XXX.XXX displays the embedded firmware version.

NOTE: Press or to exit the Product information screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?