DOCA0108EN-03

Communication Setting Menu (4/7)

Overview

The Communication setting menu allows you to set the following parameters:

  • Device address

  • Comm speed

  • Parity

The figure displays the Communication setting menu.

Communication Parameters

Parameters

Authorised Value

Factory Value

Device address

1 to 247

247

Com speed

  • 4800

  • 9600

  • 19200

  • 38400

  • Auto

19200

Parity

  • None

  • Odd

  • Even

Even

NOTE: When the communication speed is set to Auto, the parity menu is not available because the parity is adapted automatically with the speed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?