DOCA0108EN-03

Channel Summary Registers

Channel Status

Address

Register

RW

Units

Type

Range

Factory

Saved

Bit

Description

0x00C8

201

R

NA

BITMAP

NA

0x0FFF

No

Validity of each bit of alarm status:

0 = invalid

1 = valid

0x00C9

202

R

NA

BITMAP

NA

0x0000

No

 

Alarm status

0–11

0 = no alarm on channel x

1 = alarm channel x

12–15

Reserved

0x00CA

203

R

NA

BITMAP

NA

0x0FFF

No

Validity of each bit of pre-alarm status:

0 = invalid

1 = valid

0x00CB

204

R

NA

BITMAP

NA

0x0000

No

Pre-alarm status

0–11

0 = no pre-alarm on channel x

1 = pre-alarm on channel x

12–15

Reserved

0x00CC

205

R

NA

BITMAP

NA

0x0FFF

No

Validity of each bit of alarm memorized:

0 = invalid

1 = valid

0x00CD

206

R

NA

BITMAP

NA

0x0000

Yes

 

Alarm memorized

0–11

0 = no alarm memorized on channel x

1 = alarm memorized channel x

12–15

Reserved

0x00CE

207

R

NA

BITMAP

NA

0x0FFF

No

Validity of each bit of toroid status:

0 = invalid

1 = valid

0x00CF

208

R

NA

BITMAP

NA

0x0000

No

Toroid status

0–11

0 = no toroid connected on channel x

1 = toroid connected channel x

12–15

Reserved

Measurements

Address

Register

RW

Units

Type

Range

Factory

Saved

Description

0x0190

401

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 1

0x0191

402

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 2

0x0192

403

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 3

0x0193

404

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 4

0x0194

405

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 5

0x0195

406

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 6

0x0196

407

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 7

0x0197

408

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 8

0x0198

409

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 9

0x0199

410

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 10

0x019A

411

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 11

0x019B

412

R

mA

INT16U

0–60000

0x0000

No

Earth-leakage current measured in channel 12

0x019C–0x01A3

413–420

R

INT16U

0x8000

No

Reserved

0x01A4

421

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 1

0x01A5

422

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 2

0x01A6

423

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 3

0x01A7

424

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 4

0x01A8

425

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 5

0x01A9

426

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 6

0x01AA

427

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 7

0x01AB

428

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 8

0x01AC

429

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 9

0x01AD

430

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 10

0x01AE

431

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 11

0x01AF

432

R

mA

INT16U

0–60000

0x0000

No

Maximum earth-leakage current measured in channel 12

0x01B0–0x01B7

433–440

R

NA

INT16U

0x8000

No

Reserved

0x01B8

441

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 1

0x01B9

442

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 2

0x01BA

443

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 3

0x01BB

444

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 4

0x01BC

445

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 5

0x01BD

446

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 6

0x01BE

447

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 7

0x01BF

448

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 8

0x01C0

449

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 9

0x01C1

450

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 10

0x01C2

451

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 11

0x01C3

452

R

NA

INT16U

0–200

0x0000

No

Threshold percentage of measured earth-leakage current of channel 12

Parameters

Address

Register

RW

Units

Type

Range

Factory

Saved

Description

0x01F4

501

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 1

0x01F5

502

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 2

0x01F6

503

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 3

0x01F7

504

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 4

0x01F8

505

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 5

0x01F9

506

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 6

0x01FA

507

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 7

0x01FB

508

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 8

0x01FC

509

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 9

0x01FD

510

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 10

0x01FE

511

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 11

0x01FF

512

RW

mA

INT16U

30–30000

30

Yes

Alarm threshold for channel 12

0x0200

513

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 1

0x0201

514

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 2

0x0202

515

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 3

0x0203

516

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 4

0x0204

517

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 5

0x0205

518

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 6

0x0206

519

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 7

0x0207

520

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 8

0x0208

521

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 9

0x0209

522

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 10

0x020A

523

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 11

0x020B

524

RW

ms

INT16U

0–4500

0

Yes

Alarm trip delay for channel 12

0x020C

525

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 1

0x020D

526

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 2

0x020E

527

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 3

0x020F

528

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 4

0x0210

529

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 5

0x0211

530

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 6

0x0212

531

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 7

0x0213

532

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 8

0x0214

533

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 9

0x0215

534

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 10

0x0216

535

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 11

0x0217

536

RW

mA

INT16U

15–30000

15

Yes

Pre-alarm threshold for channel 12

0x0218

537

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 1

0x0219

538

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 2

0x021A

539

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 3

0x021B

540

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 4

0x021C

541

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 5

0x021D

542

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 6

0x021E

543

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 7

0x021F

544

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 8

0x0220

545

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 9

0x0221

546

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 10

0x0222

547

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 11

0x0223

548

RW

ms

INT16U

0–4500

200

Yes

Pre-alarm trip delay for channel 12

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?