Status Screens
Initialisations Screen
The screen displays the connected toroid when the device is powered on.
Toroid Detection Screen
The Toroid detection List screen displays the connected toroids when new toroid is connected.(In the above example toroid 5 was connected after initialisation).
Alarm Screen
The screen appears when only one alarm is detected.
The screen appears when alarms are detected for more than one toroid.
-
The toroids, which are not connected are not displayed.
-
The active toroids, which are not in alarm are displayed in standard black color.
-
The active toroids, which are in alarm are displayed in bold.
-
The toroids 2, 5, 10, and 12 are not connected.
-
The active toroids without alarm are 1, 3, 6, 7, 8, and 11
-
The active toroids with alarm are 4 and 9.
Pre-Alarm Screen
The screen appears when only one pre-alarm is detected.
The screen appears when alarms are detected for more than one toroid.
-
The toroids, which are not connected are not displayed.
-
The active toroids, which are not in alarm are displayed in standard black color.
-
The active toroids, which are in alarm are displayed in bold.
-
The toroids 3, 6, 8, and 10 are not connected.
-
The active toroids without alarm are 1, 2, 5, 7, 9, and 12
-
The active toroids with alarm are 4 and 11.
Selecting a Toroid
The selected toroid is highlighted in black color.