SUG_Wiser_Denmark_WSE-09

Access levels in the app

Home members can perform various tasks in the app, depending on their access level.

There are 3 access levels in the app:

  • Home owner

    NOTE: For each Home, only one Home member can be set as the Home owner.

  • Administrator

  • Common member

Function Supported Features Home owner Administrators Common members

Manage Homes and Home members

Transfer Home owner rights to another Home member

Yes

No

No

Add or delete* a Home
(*Delete the entire Home, its members and devices)

Yes

No

No

Remove a Home
(Access to the Home is removed from the user’s app, but the Home is not deleted)

Yes

Yes

No

Configure Home details

Yes

Yes

No

Add or delete Home members

Yes

Yes

No

Grant administrator access for a Home member

Yes

No

No

Receive invite notifications from a home

Yes

Yes

Yes

Manage Rooms

Add or delete Rooms

Yes

Yes

No

Name or rename Rooms

Yes

Yes

No

Manage devices

Add or delete devices

Yes

Yes

No

Configure device feature setting and schedule

Yes

Yes

Yes

Change device icon, name and location

Yes

Yes

No

Operate device

Yes

Yes

Yes

Update device firmware

Yes

Yes

No

Receive device alarm notifications

Yes

Yes

Yes

‘Device added’, ‘Device factory restored’, ‘Receive device alarm' notification

Yes

Yes

Yes

Manage Moments and Automations

Create Moments and Automations

Yes

Yes

No

Assign devices to Moments/Automations

Yes

Yes

No

Adjust device settings in Moments/Automations

Yes

Yes

No

Set Trigger conditions in Moments/Automations

Yes

Yes

No

Receive Moment/Automation trigger notifications

Yes

Yes

Yes

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.