SUG_Wiser_Denmark_WSE-09

Device LED behavior

Devices have LEDs to indicate their operating status and to confirm actions such as resetting or joining a network.

Gateway

Status

LED Indication

LED Indication Duration

Switching On/Restarting

All 3 LEDs display solid white

40 s

Connected to router (Wi-Fi)

WLAN LED displays solid white

While connected to router

Connected to router (Ethernet)

Ethernet LED displays solid white

While connected to router

Zigbee network initialized

Zigbee network LED displays solid white

While Zigbee network is available

Zigbee network open for pairing (Wi-Fi)

WLAN LED displays solid white, Zigbee network LED blinks white

While Zigbee network is open

Zigbee network open for pairing (Ethernet)

Ethernet LED displays solid white, Zigbee network LED blinks white

While Zigbee network is open

Resetting Gateway

Reset Level

User Action

LED Indication

LED Indication Duration

Level 1 reset in progress. (Restores Ethernet/WLAN settings only)

Press and hold the Reset button for 5 to 15 seconds

Ethernet/WLAN LEDs blink white.

LEDs blink once.

Level 2 reset in progress. (Upon successful reset, all configuration data, user data, and network data is deleted).

Press and hold the Reset button for more than 15 seconds

Ethernet/WLAN LEDs blink white.

LEDs blink 3 times.

Pairing

Device

User Action

LED Indication

Status

Sensors, PIR, Contact kit, Pucks, SmartPlug, Wireless dimmer, Wireless relay, Wireless battery 4 button switch

Press the push button 3 times

LED blinks orange, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a time, before turning Off.

IP camera Indoor

Plug-in the power cable to power on the device

After a few seconds LED starts blinking red for pairing.

LED glows green, when the pairing mode is complete.

IP Camera Outdoor

Plug-in the power cable to power on the device

After a few seconds LED starts blinking red for pairing.

  • LED blinks blue, when searching for Wi-Fi mode

  • LED glows blue, when connected to Wi-Fi

Resetting smart devices

Device

User Action

LED Indication

Status

Sensors, PIR, Contact kit, Pucks, SmartPlug, Wireless dimmer, Wireless relay, Wireless battery 4 button switch

Press the push button 3 times and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED starts blinks green, before turning Off.

LK FUGA® Wiser wireless socket outlet 1½ M

Status

LED Indication

Description

Setting 1 (Default state)

The Red LED glows.

  • The Red LED glows when the output is switched ON

  • The LEDs are OFF, when the output is OFF.

All the LEDs are OFF.

Setting 2

The Red LED glows

  • Red LED is ON when output is ON.

  • Green LED is ON when output is OFF.

The Green LED glows

Setting 3

All LEDs are OFF

  • All LEDs are OFF, when the output is OFF.

  • Green LED is ON when output is OFF.

Green LED is glows

Setting 4

All LEDs are OFF

There will be no LED indication in any case of the output state.

NOTE: Above settings are done in the app.

Wiser Radiator Thermostat

Normal use

State

User action

Left LED

Centre LED

Right LED

Duration

Boost up Twist the cap in the + direction Not active Not active Solid for 5 seconds.
Boost down Twist the cap in the — direction Not active Not active Solid for 5 seconds.

Head calibration

State

User action

Left LED

Centre LED

Right LED

Duration

Start up Insert the batteries Single quick flash
Opening the valve Automatic upon inserting batteries OR Twist and hold the cap in + direction Not active Not active Solid until the valve is open
Ready to install on the valve The radiator thermostat is ready to install when the valve is fully open Red and Blue: Flash for up to 5 minutes

Orange solid= not joined | Green solid= joined

Closing the valve Twist and hold the cap in the — direction for 2 seconds Not active Not active Solid until the valve is closed
Joining Twist and hold the cap in the + direction for 3 seconds Not active Not active Pulses for up to 2 minutes
Join success   Not active Not active Solid for 5 seconds
Failed to join If no network is found after 2 minutes Not active Not active Flashes for 5 seconds

Error state

State

User action

Left LED

Centre LED

Right LED

Duration

Low battery Twist the cap in the + direction Not active Not active Solid for 1 second (Repeated each hour)
Critical battery Twist the cap in the — direction Not active Not active Fast flash for 5 seconds (Repeated each minute)
No signal Twist the cap in the + direction to start a boost Not active Not active Fast flash for 5 seconds (Repeated)
No signal Twist the cap in the — direction to start a boost Not active Not active Fast flash for 5 seconds (Repeated)
No network Twist the cap in the + or — direction to start a boost Not active Not active Solid with fade-out after 2 seconds. In this event, the radiator thermostat has not joined the system and must either join the Gateway gateway or re-installed.

Smoke Alarm Battery/ Wiser Smoke Alarm 230 V

Pairing

User Action

LED Indication

Status

Press the Setup/Reset button 3 times

LED blinks yellow, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off.

Resetting

User Action

LED Indication

Status

Press the Setup/Reset button 3 times and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED starts blinks green before turning Off.

Operating

Operating Mode Standby LED Alarming Sound Duration

Normal mode / Standby mode

Blinks every 48 s

OFF

Alarm Mode

Local Alarm *

Blinks every 1 s

3 beeps every 4 s

Interconnected alarm

OFF

3 beeps every 4 s

Test mode

1 blink every 1 s

3 beeps every 4 s

Until Test/Hush button is released

RF interconnection test

OFF

Continuous 3 beeps every 4 s

25 s

Hush mode

Blinks every 8 s

OFF

10 min

Low battery mode

Blinks every 48 s

1 beep every 48 s

End of life: replace smoke alarm

Fault mode

2 blinks every 48 s

2 beeps every 48 s

Until fault has been cleared

Snooze Mode

Low battery

Blinks every 24 s

OFF

10 hrs

Fault

2 blinks every 24 s

OFF

10 hrs

Alarm memory

Blinks every 48 s

OFF

10 hrs

NOTE: For all the operating modes, LED blinks Red.

* Local smoke alarm all Red LEDs blink and for Local temperature alarm only Standby Red LED blinks.

PowerTag Energy

Behavior Communication indicator light

PowerTag Energy switched off.

PowerTag Energy is searching for a Gateway in pairing mode.

PowerTag Energy is in identification mode.

PowerTag Energy is in network. Normal communication with the Gateway .

Occasional loss of communication.

Loss of communication with the Gateway .

Internal error detected.

Wiser Adapter

Pairing

User Action

LED Indication

Status

Press the operation button 3 times within 2 seconds.

LED blinks red, once per second.

Pairing mode is active for 180 seconds. When pairing is completed, LED glows red if the operation button is turned On before you start pairing, else the LED turns Off.

Resetting

User Action

LED Indication

Status

Press the operation button 3 times within 2 seconds and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED blinks red indicating pairing mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.