SUG_Wiser_Denmark_WSE-09

Overview of the Wiser™ system

The Wiser system provides an easy, convenient and flexible solution for controlling home devices.

The Wiser gateway is the center of the system, processing control requests and status reports for connected Wiser devices.

Use the Wiser by SE app to set up the Wiser system, control Wiser devices and receive notifications.

With a personal account and the Wiser by SE app on a mobile phone/tablet, users can control Wiser devices in their home from any location where internet is available for both mobile phone/tablet and the Wiser gateway.

Within the home, the devices, such as, LK FUGA® Wiser wireless battery 4 button switch, LK FUGA® Wiser wireless double relay, LK FUGA® Wiser wireless dimmer can be used to control the Wiser system.

TIP: You can follow the LK Welcome web page and Catalog for more information on the product and features.

For LK Welcome Web Page: Visit https://www.lk.dk/professionel/produktoversigt/intelligente-systemer/wiser-smart-home/
For LK Catalog: Visit https://www.lk.dk/produkter?iid=384

Device groups

Operate identical Wiser devices together, either from the local control on one of the devices or by using the Wiser app.

Use the Group feature in the Wiser app to combine many identical devices and operate them as one unit. For example, create a group of three Wiser light switches for multi-way operation.

Device groups Control assistance
Lights, Switches/Dimmers Lighting and dimming
Shutters/Blinds/Curtains Motorized shutters and blinds
Sockets/Adapters Electric supply
Heating Temperature
Cameras Security and privacy
Energy Monitors power consumption
Safety and Sensors Smoke alarm, Room occupancy, window/door open or close, temperature and humidity, water leakage

Operate identical Wiser devices together, either from the local control on one of the devices or by using the Wiser Mobile app.

The following category of devices are available to provide convenient control of:

  • lighting and dimming

  • motorised shutters and blinds

  • heating

Sensors are also available to record and report the following:

  • room occupancy

  • ambient light level

  • window/door open or close

  • temperature and humidity

  • water leakage

  • energy management

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.