SUG_Wiser_Denmark_WSE-09

Light switches

LK FUGA®Wiser Wireless Double Relay

Controls the lights in a room, or automatically switch lights On or Off in response to a specified condition or event.

LK product catalog

Instruction Sheet (PDF)

Wiser Wireless Relay for Build in (Puck)

Converts compatible mechanical push-button switches into smart switches. Connect up to 10 compatible mechanical push buttons.

NOTE: Mechanical push buttons must be certified for use in 220–240 V AC applications.

LK product catalog

Instruction Sheet (PDF)

Device User Guide

LK FUGA® Wiser Wireless PIR with Relay

Detects moving heat sources (e.g. persons) and can switch on ohmic, inductive or capacitive loads for a adjustable overtravel time.

LK product catalog

Instruction Sheet (PDF)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.