SUG_Wiser_Denmark_WSE-09

Pairing to other devices

You can combine compatible devices into a group so that when one device in the group is operated, the other devices also operate. This can be done independently of the Gateway and app.

NOTE: You can only operate paired devices from the physical buttons on a device and not from the app. However, any device function and setting in the app remain unaffected by pairing devices together.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.