SUG_Wiser_Denmark_WSE-09

Removing a Wireless battery switch from a Room Control group

Remove the link between Wireless battery switch and other devices when the remote control operation is no longer needed.
  1. (See A, B) Short press the button (1) at top-left of the device (A) 3 times then press and hold the button for 6 seconds.
    The status LED (B) blinks green after 6 seconds.
    NOTE: The pairing between the Wireless battery switch and compatible devices is removed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.