SUG_Wiser_Denmark_WSE-09

Compatible devices for Room Control

Selected devices can be used in a Room Control group.

Lighting control devices

Device name

Commercial reference number(s)

LK FUGA® Wiser wireless double relay

545D6514, 545D0514

LK FUGA® Wiser wireless dimmer

545D6102, 545D0102

Wiser wireless relay for build in (Puck)

550B1011

Wiser wireless dimmer for build in (Puck)

550B1012

Shutter control devices

NOTE: Shutter control devices can only be combined with other shutter control devices. Do not mix shutter and lighting applications.

Device name

Commercial reference number(s)

Wiser wireless shutter control for build in (Puck)

550B1013

Control devices

Device name

Commercial reference number(s)

LK FUGA® Wiser wireless battery 4 button switch

550D6001, 550D0001

LK FUGA® Wiser wireless double relay

545D6514, 545D0514

LK FUGA® Wiser wireless double dimmer

(Only the upper two buttons can be used for room control. The lower two buttons 1 and 2 are scenes for local control)

545D6102, 545D0102

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.