SUG_Wiser_Denmark_WSE-09

Energy device

PowerTag Energy

PowerTag E (hereinafter referred as PowerTag) is a compact, robust, and easy-to-install wireless communication energy sensor. It is used together with the Gateway/Hub to collect information from every equipped circuit to identify the energy consumption of each connected load. It is designed specifically to manage energy consumption for new and existing residential installations. It monitors and measures energy and power in real-time, and also provides complete visibility of power transfer between power source and loads.

LK Product Catalog (RM920)

LK Product Catalog (RM921)

LK Product Catalog (RM922)

LK Product Catalog ((R9M41)

LK Product Catalog (R9M42)

LK Product Catalog (R9M60)

Instruction Sheet (PDF)- PowerTag Resi9 M63

Instruction Sheet (PDF)- PowerTag Resi9 F63

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.